Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20974
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

How the system can be simplified with the Roll to Roll dedicated inverter?
Category : 

Answer

When the winding ratio is large, the control according to the winding diameter is required. The upper controller has measured the winding diameter and created the command for the inverter. With the Roll to Roll dedicated machine, the control that have been performed in combination with the controller can be achieved by the inverter alone. Construction of small and medium size systems has become much more simple.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries