FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800
FAQ
FR-A800
When Pr.820: Speed control P gain 1 is set to 0%, how does it affect the response?
- Category :
Answer
Since the lower limit has been internally set, the setting value of 3 % or less is recognized as 3%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800