FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > PLC function
FAQ
PLC function
What happens with the data when SD1236, 1237, and 1238 overflow?
- Category :
Answer
The maximum values are kept. The values are not cleared to zero.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800