FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Gain adjustment under the speed control
FAQ
Gain adjustment under the speed control
What happens with the response when Pr.820 is set to 0%?
- Category :
Answer
Since the lower limit has been internally set, 3% or less is recognized as 3%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800