FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F500 > Use of the DC reactor
FAQ
Use of the DC reactor
Can I use the DC reactor supplied with the FR-A500L/FR-F500L for the FR-A800/F800?
- Category :
Answer
It can be used in terms of the specifications. However, it is recommended to update the reactor and inverter at the same time because the DC reactor was manufactured over ten years ago.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800