FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > RS-485 and analog input
FAQ
RS-485 and analog input
When applying the frequency command with the FR-D700, is there any difference between the RS-485 and analog input?
- Category :
Answer
The time from when the frequency command is applied until it is reflected on the operation of the motor is different. For the analog input, the multiple analog input terminals such as second terminal and fourth terminal are switched and read sequentially. Therefore, the response of the RS-485 is improved compared to the analog input.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700