FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Sine wave filter
FAQ
Sine wave filter
When using Real sensorless vector control, can I use the sine wave filter?
- Category :
Answer
The sine wave filter can be applied only under V/F control. When Pr.72 PWM frequency selection is set to 25, V/F control is set automatically. The applicable output frequency is 60 Hz or less.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- FR-A800, FR-A700