FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > The number of output terminals
FAQ
The number of output terminals
Is the number of output terminals and the terminal function selection same as the F700P?
(For F700P: RUN, SU, IPF, OL, FU, ABC)
(For F700P: RUN, SU, IPF, OL, FU, ABC)
- Category :
Answer
The number of terminals: There are the same output terminals as F700P and the following terminals (2 points) are added. Safety: SO, SOC *The terminals SO and SOC are dedicated to the safety. Functions cannot be changed as other terminals.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800