FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > SW1DND-FRC2 (FR Configurator2)
FAQ
SW1DND-FRC2 (FR Configurator2)
The communication error (ES:0x010a4001) occurs in Developer although the communication of FR Configurator2 can be performed. What are the possible causes for this?
- Category :
Answer
Check the setting value of Pr.414 (PLC function operation selection) and if the initial value: 0 (PLC function disabled) is set, set "1" or "2" and enable the PLC function.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR-A800, FR-F800, option