Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21092
  • Release Date : 2018/08/22 16:25
  • Print

DC reactor

Can I use the DC reactor 75K or higher enclosed with the A700/F700P?
Category : 

Answer

It can be used since the specifications are the same. Note that the warranty period and expected lifespan for the A700/F700P are inherited.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?