FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > USB
FAQ
USB
What is USB used for?
- Category :
Answer
The mini B connector is used for connecting with FR Configurator2. A USB memory device can be connected to the A connector (host) to save parameters or trace data or to copy parameters from one A800/F800 to another A800/F800. Parameters can be copied from one to another through a USB cable connected to the A connectors.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800