FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > 24 VDC power supply
FAQ
24 VDC power supply
What will be available if power is supplied to the 24 VDC power supply terminal?
- Category :
Answer
Power is supplied only to the control power supply, and thus this enables communication, parameter setting through the operation panel or an USB memory device, and operation check of the input/output terminals. * The 24 VDC power supply turns OFF when the main circuit power supply is ON.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800