Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21101
  • Release Date : 2018/08/22 16:25
  • Print

Multiple rating

What are the advantages by the multiple rating?
Category : 

Answer

By setting the operating condition, such as load level and surrounding air temperature, according to the application, the inverter capacity may be lowered compared to the conventional model depending on the conditions, allowing installation space to be minimized and costs reduced.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?