FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-RC
FAQ
FR-RC
What is the setting values of Pr.30 and Pr.70 when the FR-RC is connected?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > Options
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Pr.30 = "1" and Pr.70 = "0".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ