FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-HC2
FAQ
FR-HC2
What is the cable gauge of the inrush current limit resistor (FR-HCR2) of the FR-HC2?
- Category :
Answer
It is 0.88 mm2 (AWG18), and 0.3 mm2 (AWG24) for the thermostat.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- Option