Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21160
  • Release Date : 2018/08/22 16:26
  • Print

Vector control

I am planning to perform Vector control with the FR-A700 and SF-V5RU together. For the wiring with the thermal protector, a resistor of 2 W 1 k? is installed. When using the external power supply with the sink logic, where should be the resistor installed?
Category : 

Answer

Install the resistor between the terminals PC and OH.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries