FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Brake sequence function
FAQ
Brake sequence function
Can the operation test of the brake sequence function be performed without connecting a motor?
- Category :
Answer
It can be performed by setting Pr.292 (Automatic acceleration/deceleration) to "8" and Pr.279 (Brake opening current) to 0%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700