FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Instruction code execution request of CC-Link communication
FAQ
Instruction code execution request of CC-Link communication
When 0 (occupies one station: A5NC compatible) is set to Pr.544 (CC-Link extended setting), if the bits of frequency setting command RYD, RYE, and instruction code execution request RYF are turned ON simultaneously, which instruction is executed?
- Category :
Answer
Only one instruction is executed. The instruction to be executed is not fixed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700