FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Monitor code of CC-Link communication
FAQ
Monitor code of CC-Link communication
When Pr.37 (Speed display) and Pr.144 (Speed setting switchover) are changed, does the monitor with the code: H01 (output frequency) switch to rotation speed or machine speed display?
- Category :
Answer
The monitor with the code H01 switches by changing Pr.37 and Pr.144.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700