FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Model selection
FAQ
Model selection
When driving the motor of 132 kW/400 V under Advanced magnetic flux vector control, which inverter model should I use?
- Category :
Answer
Use the FR-A740. Basically, select the capacity according to the calculation result of "rated inverter output current ? rated motor current × 1.1".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700