FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Proportional band of multiple inverters
FAQ
Proportional band of multiple inverters
I want to perform proportional band of three inverters by changing the speed of one inverter. How should I input the inverter analog output to the second inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
By importing the operation frequency from the AM terminal (analog output) of the first inverter to the FR-FH (ratio setter), the operation command which is proportional to other three inverters can be sent.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700