FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Frequency setting signal
FAQ
Frequency setting signal
I want to set 0 Hz for 4 mA and 50 Hz for 20 mA while the current 4 to 20 mA is input to terminal 4. Which parameters should I set?
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
Set C5 (Pr.904) (Terminal 4 frequency setting bias frequency) to 0 Hz and Pr.126 (Terminal 4 frequency setting gain frequency) to 50 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700