FAQ


FAQAbout Products
 
 - FAQ > Drive Products > Inverters-FREQROL > Rated frequency setting
FAQ
Rated frequency setting
      When the spindle motor with 200 Hz rated frequency is used, "OL" (overload) is displayed at 4 to 5 Hz and the speed does not increase. 
How should I configure the setting?
  How should I configure the setting?
- Category :
- 
      - FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
 
Answer
    Check that Pr.3 (Base frequency) is set to "200 Hz". 
Adjust Pr.0 (Torque boost) as necessary.
    Adjust Pr.0 (Torque boost) as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700