FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Specifications
FAQ
Specifications
The specification of the inverter is three-phase 200 V power input. Can I drive the three-phase 200 V motor by inputting single-phase 200 V?
- Category :
Answer
It can be driven by connecting single-phase 200 V to the terminals R and S.
In this case, the load current must be one-third or less of the inverter rated current.
In this case, the load current must be one-third or less of the inverter rated current.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700