FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency
FAQ
Frequency
When the output frequency is increased from 60 Hz to 80 Hz, how much does the motor torque decreases?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
When the torque is supposed as 100% at 60 Hz, the torque becomes 75 % at 80 Hz.
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700