FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency
FAQ
Frequency
When the output frequency is increased from 60 Hz to 80 Hz, how much does the motor torque decreases?
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
When the torque is supposed as 100% at 60 Hz, the torque becomes 75 % at 80 Hz.
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
(Under V/F control, the torque decreases when the frequency exceeds 60 Hz because the voltage over a certain limit cannot be output.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700