FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Start command
FAQ
Start command
I want to give a start command for the inverter from "NET" and frequency command from the potentiometer connected to the terminals 10, 2, and 5.
Which parameters should I set?
Which parameters should I set?
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
Set Pr.338 (Communication command source) to "0" to give a start command from "NET". Set Pr.339 (Speed command source) to "1" to make a frequency setting from the "external" input.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700