FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Switching External operation, PU operation
FAQ
Switching External operation, PU operation
I want to switch the operation from External operation to PU operation while running the External operation.
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Setting Pr.79 (Operation mode) to "6" sets the switchover mode. Pressing the "PU/EXT" key on the operation panel during External operation switches the mode to the PU operation mode and enables the PU operation.
(The start signal (forward/reverse) and frequency setting of the External operation are inherited.)
The operation mode can be switched from PU operation mode to External operation as well.
(The start signal and frequency setting of the PU operation are not inherited.)
(The start signal (forward/reverse) and frequency setting of the External operation are inherited.)
The operation mode can be switched from PU operation mode to External operation as well.
(The start signal and frequency setting of the PU operation are not inherited.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700