FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > RS-485 communication
FAQ
RS-485 communication
I want to operate the inverter in RS-485 communication.
I have input forward rotation command with the communication, but the "RUN" LED on the panel blinks and the inverter does not operate.
What are the possible causes for this?
I have input forward rotation command with the communication, but the "RUN" LED on the panel blinks and the inverter does not operate.
What are the possible causes for this?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Blinking of the "RUN" LED on the panel suggests that the frequency command may not be input.
Create a frequency setting data as for the forward rotation command and send it to the inverter.
For how to format the data, refer to the Instruction Manual (Applied).
Create a frequency setting data as for the forward rotation command and send it to the inverter.
For how to format the data, refer to the Instruction Manual (Applied).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700