FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > FR-PA07
FAQ
FR-PA07
When Pr.79 (Operation mode) is set to "3", and using the option FR-PA07 and external terminals, does the RUN key on the FR-PA07 work?
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
When Pr.79 is set to "3", since the start command is in the External operation mode, the RUN key of FR-PA07 does not work.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700