FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Number of stations that can be set in FR Configurator
FAQ
Number of stations that can be set in FR Configurator
I want to connect FR-Configurator (FR-SW3-SETUP-WJ) setup software using the USB.
It seems like station numbers 0 to 31 can be set. Can I arrange them individually?
It seems like station numbers 0 to 31 can be set. Can I arrange them individually?
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
The station numbers that can be set differ depending on the version of FR-Configurator (FR-SW3-SETUP-WJ) setup software.
For Ver.2.00 or later, station numbers 0 to 31 can be individually set.
For Ver.2.00 or later, station numbers 0 to 31 can be individually set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700