FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Saving parameter with FR-Configurator
FAQ
Saving parameter with FR-Configurator
Can I reduce the size of the parameter data before saving it by using FR Configurator (FR-SW3-SETUP-WJ)?
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
When FR Configurator (FR-SW3-SETUP-WJ) is saved as a file from the menu, the extension is "me3".
The size of this fie will be large since device settings and graph data are included as well as parameters.
The file size can be reduced when only the parameter list is saved from "File" - "Export" with the extension "pr3".
The size of this fie will be large since device settings and graph data are included as well as parameters.
The file size can be reduced when only the parameter list is saved from "File" - "Export" with the extension "pr3".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700