FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > NET operation mode
FAQ
NET operation mode
I want to perform communication with the FX series programmable controller and start operation in the NET operation mode at power-ON.
Even though Pr.340 (Communication startup mode selection) is set to "10" and Pr.79 (Operation mode selection) is set to "0", the inverter starts up not in the NET operation mode but in the PU operation mode.
Even though Pr.340 (Communication startup mode selection) is set to "10" and Pr.79 (Operation mode selection) is set to "0", the inverter starts up not in the NET operation mode but in the PU operation mode.
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Normally, the inverter starts up in the NET operation mode at power ON when Pr.340 is set to "10" and Pr.79 is set to "0".
When it starts up in the PU operation mode, the input terminal where X65 (PU-NET operation switchover) signal is assigned may be ON.
Check the terminal assignment and check that the signal is not ON.
Or, change the setting of Pr.340 to "1" and check that the inverter starts up in the NET operation mode.
When it starts up in the PU operation mode, the input terminal where X65 (PU-NET operation switchover) signal is assigned may be ON.
Check the terminal assignment and check that the signal is not ON.
Or, change the setting of Pr.340 to "1" and check that the inverter starts up in the NET operation mode.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700