FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Electromagnetic contactor
FAQ
Electromagnetic contactor
Can I start and stop the inverter with the electromagnetic contactor (MC) installed on the primary side of the inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
It is not recommended to start and stop the inverter with the electromagnetic contactor (MC). This will accelerate the deterioration (due to the inrush current at startup) of the internal inverter parts.
If the electromagnetic contactor is used to start and stop the inverter more than three times a day, use the terminals STF and SD instead.
If the electromagnetic contactor is used to start and stop the inverter more than three times a day, use the terminals STF and SD instead.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700