FAQ


FAQAbout Products
 - FAQ > Drive Products > Inverters-FREQROL > Capacity selection
 
FAQ
Capacity selection
      How can I select the inverter capacity when using a motor?
    
  - Category :
 - 
      
- FAQ > Drive Products > Inverters-FREQROL
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
 
 
Answer
    Select the inverter capacity so that the rated output current of inverter ? rated motor current × 1.1.
  
    - Product Name
 - Inverter, magnet motor drive
 
- Product Category
 - Inverter
 
- Series
 - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700