FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Brake resistor
FAQ
Brake resistor
Is only one resistor used for the high-duty brake resistor FR-ABR-15K (inverter option)?
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
Use two resistors for the high-duty brake resistor FR-ABR-15K. (Connect two resistors of 18 ? in parallel.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700