FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Pulse change
FAQ
Pulse change
When the output frequency is output from the terminal FM, the value stops when the maximum frequency is reached.
The pulse is counted and displayed.
When the frequency is 60 Hz, 1440 pulses are output. Can I change the number of pulses at 60 Hz?
The pulse is counted and displayed.
When the frequency is 60 Hz, 1440 pulses are output. Can I change the number of pulses at 60 Hz?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
When the pulse is counted and displayed, 1440 pulses are output with the frequency of the inverter is 60 Hz. Since these pulses are limited to 2400 pulses, and the value stops when the maximum frequency is reached.
The number of pulses at 60 Hz can be changed with Pr.55 (Frequency monitoring reference) as the frequency for 1440 pulses.
The number of pulses at 60 Hz can be changed with Pr.55 (Frequency monitoring reference) as the frequency for 1440 pulses.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700