FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Wiring the terminal
FAQ
Wiring the terminal
I use the 24 VDC power supply of the terminal PC with a 24 VDC relay across the terminals PC and RUN and terminals across SD and SE shortened.
Is there any problem with the wiring?
Is there any problem with the wiring?
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
There is no problem with the wiring.
Keep the rating (24 VDC, 0.1 A) of the terminal PC.
Keep the rating (24 VDC, 0.1 A) of the terminal PC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700