FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-PA02
FAQ
FR-PA02
Can I use the operation panel used in the FR-E500 by setting Pr.146 (Built-in potentiometer switching) to "0"?
- Category :
Answer
The operation panel FR-PA02 requires the optional FR-E5P (control panel rear cover and adapter set) and connection cable FR-CB20□.
Check that Pr.146 (Built-in potentiometer switching) is set to "0".
Otherwise, the built-in potentiometer of the FR-PA02 cannot be used.
Check that Pr.146 (Built-in potentiometer switching) is set to "0".
Otherwise, the built-in potentiometer of the FR-PA02 cannot be used.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ