FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Countermeasure against harmonics
FAQ
Countermeasure against harmonics
When the FR-F520-15K high power factor converter is used against harmonics, what will the harmonics generation rate be?
I have to submit the harmonics generation device manufacturer application form. How should I create it?
I have to submit the harmonics generation device manufacturer application form. How should I create it?
- Category :
Answer
When the high power factor converter is installed, you can use the conversion coefficient of K5 = 0 for calculation.
In accordance with the harmonic suppression guidelines, you can assume that harmonic current is not generated.
Note that the harmonics generation device manufacturer application form is required only when equipment that contains a dedicated circuit configuration not defined in the guideline is used. It is not necessary for general-purpose inverters.
In accordance with the harmonic suppression guidelines, you can assume that harmonic current is not generated.
Note that the harmonics generation device manufacturer application form is required only when equipment that contains a dedicated circuit configuration not defined in the guideline is used. It is not necessary for general-purpose inverters.
- Product Name
- Inverter, magnet motor drive
- Series
- Others