FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200 > Surge voltage of 400 V motor
FAQ
Surge voltage of 400 V motor
To upgrade the existing facilities, what is necessary in addition to the inverter for when 400 V motor and inverter are used.
Is there possibility of motor burnout since the motor is not upgraded this time?
Is there possibility of motor burnout since the motor is not upgraded this time?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A024
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A200
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A100
Answer
When the wire between the 400 V inverter and motor is long (20 m or longer), surge voltage occurs momentarily. This voltage is as two or more times as the DC voltages converted by the inverter (400 VAC × √2 = 565 VDC), and is 1000 VDC or higher.
Since this voltage can deteriorate insulation of the motor:
1. Use an insulation-enhanced motor.
2. Attach the surge voltage suppression filter (FR-ASF-H).
Consider the above countermeasures.
Since this voltage can deteriorate insulation of the motor:
1. Use an insulation-enhanced motor.
2. Attach the surge voltage suppression filter (FR-ASF-H).
Consider the above countermeasures.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024, FR-E500, FR-A100, FR-F500, FR-A200, FR-A500, FR-V200