FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Dealing with Err.
FAQ
Dealing with Err.
"Err." is displayed on the parameter unit.
It does not disappear by turning the power supply OFF or disconnecting the parameter unit cable connector from the inverter. What is the possible cause?
It does not disappear by turning the power supply OFF or disconnecting the parameter unit cable connector from the inverter. What is the possible cause?
- Category :
Answer
The following causes are probable for persistent Err. display:
1. The terminals RES and SD are always short-circuited.
2. Operation panel contact or operation panel itself is faulty.
3. Inverter is faulty.
If the inverter can be operated from the external source while "Err." is displayed on the operation panel, the cause (2) is highly probable. Check connection between the inverter and operation panel again.
If the inverter cannot operate, the cause (1) or (3) is highly probable.
1. The terminals RES and SD are always short-circuited.
2. Operation panel contact or operation panel itself is faulty.
3. Inverter is faulty.
If the inverter can be operated from the external source while "Err." is displayed on the operation panel, the cause (2) is highly probable. Check connection between the inverter and operation panel again.
If the inverter cannot operate, the cause (1) or (3) is highly probable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500