FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200 > Meaning of OL display (2)
FAQ
Meaning of OL display (2)
While the inverter is operating with the externally set torque limit, is "OL" displayed even when the inverter is operating within the rated torque and below the limit?
- Category :
Answer
Yes.
"OL" is displayed under speed control whenever the torque limit is reached without regard to the rated torque.
"OL" is displayed under speed control whenever the torque limit is reached without regard to the rated torque.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200