Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21448
  • Release Date : 2018/08/22 16:27
  • Print

Meaning of OL display (2)

While the inverter is operating with the externally set torque limit, is "OL" displayed even when the inverter is operating within the rated torque and below the limit?
Category : 

Answer

Yes.

"OL" is displayed under speed control whenever the torque limit is reached without regard to the rated torque.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries