FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Meaning of OL display
FAQ
Meaning of OL display
"OL" is displayed on the operation panel. What does it mean?
- Category :
Answer
"OL" stands for "overload".
Whenever current of 150% or more of the inverter rated current flows, "OL" is ON.
If you continue operation with "OL" is displayed, a thermal trip is triggered. Therefore you need to reduce the load.
Whenever current of 150% or more of the inverter rated current flows, "OL" is ON.
If you continue operation with "OL" is displayed, a thermal trip is triggered. Therefore you need to reduce the load.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200