FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200 > Rotations per minute vary
FAQ
Rotations per minute vary
When the parameter unit is connected to the FR-V220-5.5K the rotations per minute is 843, but it increases to 847 when the parameter unit is disconnected.
Why do the rotations per minute vary?
Why do the rotations per minute vary?
- Category :
Answer
It is considered that conditions including the power supply and noise change whether the parameter unit is connected or disconnected, influencing the analog input command signals.
Do not disconnect the parameter unit during operation or use the digital input command unit (FR-VPC option).
Do not disconnect the parameter unit during operation or use the digital input command unit (FR-VPC option).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200