FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-V200 > Connecting potentiometer
FAQ
Connecting potentiometer
I have two FR-V220E-5.5K units and I want to use them with a single external potentiometer for variable speed control.
Do you have a connection example?
Do you have a connection example?
- Category :
Answer
Connect the external potentiometer to the terminals 10, 2, and 5 of the first inverter (be sure to connect the variable terminal to the terminal 2). Connect the terminals 2 and 5 of the first inverter to the terminals 2 and 5 of the second inverter using wires. Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-V200