Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21467
  • Release Date : 2018/08/22 16:27
  • Print

Parameter No.79 (Operation mode)

I use the inverter FR-E500 and set Pr.79 (Operation mode) to "3" to use the potentiometer on the inverter.
When the multi-speed command is input, multi-speed operation is enabled. Can I cancel this?
Category : 

Answer

You cannot cancel multi-speed command input.

When the multi-speed command is input from the terminal, you cannot use the potentiometer.
Use the inverter so that the multi-command is not input (not turned ON) from the terminal.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?