FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Using dedicated motor
FAQ
Using dedicated motor
I use the FR-A024-0.75KP with single-phase input.
I also use a three-phase input 2P 0.6 kW dedicated motor.
I want to draw the maximum ability of the motor. Can I adjust the motor constants of the inverter for this purpose?
In concrete, I want to adjust the motor resistance and reactance constant.
Are there any other items that I can set?
I also use a three-phase input 2P 0.6 kW dedicated motor.
I want to draw the maximum ability of the motor. Can I adjust the motor constants of the inverter for this purpose?
In concrete, I want to adjust the motor resistance and reactance constant.
Are there any other items that I can set?
- Category :
Answer
Since the inverter power supply uses the single-phase input, you cannot use a 0.75K inverter with a 0.6 kW motor to draw the maximum ability of the motor.
To do this, you need a 1.5K inverter.
You cannot adjust individual motor constants of the inverter such as the motor resistance and reactance constant.
To do this, you need a 1.5K inverter.
You cannot adjust individual motor constants of the inverter such as the motor resistance and reactance constant.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024