FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Inverter analog output
FAQ
Inverter analog output
I want to input two channels each from the inverters FR-B-37K (with parameter unit), FR-B-5.5K (with parameter unit), and FR-B-1500 (with parameter unit) (all based on the FR-A220E) to the programmable controller as the analog monitor. Which option do I need? Or, can I do this without any option?
- Category :
Answer
Since the inverter has only one voltage output (10 VDC) from terminal AM as the analog monitor, use the FR-EPA or FR-EPE option if you need two channels.
The FR-EPA and FR-EPE options have the voltage output (5/10 VDC) × 1 and current output (1 mA DC) × 1 that can be used simultaneously.
Use one of the above options, and determine if you use two channels from the option or one channel each from the inverter and option.
The FR-EPA and FR-EPE options have the voltage output (5/10 VDC) × 1 and current output (1 mA DC) × 1 that can be used simultaneously.
Use one of the above options, and determine if you use two channels from the option or one channel each from the inverter and option.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-B